i.MXRT1064 EVK PCB file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1064 EVK PCB file

1,956 Views
msbala
Contributor I

Dear NXP Deam,

Kindly help me on this customer support.

 

We want to study the i.MXRT1064 EVK PCB file which is in Allegro tool.

We want to open it in Altium, for that ASCII file generated from Allegro is required.

Please help to provide that as well.

 

EVK LINK

https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/mimxrt1064-evk-...

Thanks 

Bala

Labels (1)
0 Kudos
Reply
5 Replies

1,749 Views
zulu1877
Contributor I

Dear NXP Team,

 

Im in exactly the same situation,

I use altuim only, could i please get a copy of the files to import please?

  

EVK LINK

https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/mimxrt1064-evk-...

 

Thanks 

Nick

0 Kudos
Reply

1,749 Views
Yuri
NXP Employee
NXP Employee

Hello, zulu1877@gmail.com !

 Is it possible for You to create request ?

Support | NXP 

Regards,

Yuri.

0 Kudos
Reply

1,749 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You directly the PCB file, which can be imported in Altium.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply

1,745 Views
MarkDudley
Contributor I

Yuri would it be possible for me to get these files as well?

0 Kudos
Reply

1,733 Views
Yuri
NXP Employee
NXP Employee

@MarkDudley 
Hello,

   Is it possible for You to create request ?

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

~Yuri.

 

0 Kudos
Reply