i.MX8MN power down sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8MN power down sequence

跳至解决方案
1,193 次查看
justin_hsieh
Contributor II

Dear Team,

We have observed that some power-down timing results do not meet the SoC's requirements. According to the specification, the power-down timing range must be between 0 and 10 ms. However, our measurement results did not meet this specification.

As far as I know, the power-down behavior will depend on the capacitor value and loading on the PCBA, which may explain why the timing range specified in the document cannot be met by all products. Would a failure in power-down timing have any impact on the product? Could we ignore the failures?

Here are the test results.

T1. Delay from PHY 1.2 V off to digital 2.5 V and 3.3 V off, the test results are -0.43ms~-0.3ms.

T3. Delay from NVCC_DRAM off to digital 1.8 V off, the test results are -0.18ms~-0.14ms.

T4. Delay from digital 1.8 V off to analog 1.8 V off, the test results are -0.31ms~-0.19ms.

T5. Delay from analog 1.8 V off to VDD_SOC off, the test results are -34.9us~-31.1us.

T9. Delay from VDD_SNVS_0P8 off to NVCC_SNVS_1P8 off, the test results are -3.97us~-2.53us.

 

justin_hsieh_0-1736234757427.png

justin_hsieh_1-1736234776313.png

Please provide recommendations.

 

0 项奖励
回复
1 解答
1,097 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The understanding of the customer is correct. If PCA9450 is used for i.MX8MN application, the measurement result should be fine because all power rails will be discharged completely by the PMIC.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,157 次查看
justin_hsieh
Contributor II

Hi Rita,

This is the data measured on our design.

Will there be any risks if we cannot meet the power-down requirement?

 

0 项奖励
回复
1,098 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The understanding of the customer is correct. If PCA9450 is used for i.MX8MN application, the measurement result should be fine because all power rails will be discharged completely by the PMIC.

0 项奖励
回复
1,148 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I will confirm it .

0 项奖励
回复
1,159 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using? NXP reference board or the board you design yourself?

0 项奖励
回复