i.MX8MM operating points

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM operating points

Jump to solution
7,177 Views
pierluigi_p
Senior Contributor I

Dear NXP team,

in the file imx8mm.dtsi, the opp-table reports the same 3 operating points documented in tabled 10 of the SoC datasheet: 1.2, 1.6 and 1.8 GHz

However, in the file clk-pll14xx.c, the table imx_pll1416x_tbl reports also additional clock frequencies.

Can these additional frequencies be introduced in the opp-table to farther reduce the clock frequency ?

If yes, which values should be used for the properties opp-microvolts, opp-supported-hw, clock-latency-ns ?

Thanks

Best Regards

Pier

0 Kudos
Reply
1 Solution
7,143 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @pierluigi_p 

Have sent your the patch.

View solution in original post

0 Kudos
Reply
10 Replies
7,144 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @pierluigi_p 

Have sent your the patch.

0 Kudos
Reply
5,607 Views
PetersonJA68
Contributor I

Was the patch mentioned here ever provided publicly?  We are working on a new device using the iMX8MM and are interested in running at operating points below 1.2 GHz.

0 Kudos
Reply
6,519 Views
m_karabela
Contributor I
I would love to see this patch. I'm interested in lowest possible power consumption of imx8mm.
Can you share it?
0 Kudos
Reply
6,667 Views
dev_pcs
Contributor I

@Zhiming_Liu can you send me also the patch?

0 Kudos
Reply
6,767 Views
VilleS
Contributor I
Can you share the patch publicly also?
0 Kudos
Reply
7,079 Views
jxb4256
Contributor II

Can you please send this patch to me too?

0 Kudos
Reply
7,136 Views
pierluigi_p
Senior Contributor I

Thanks @Zhiming_Liu,

one last question: can I share the patch with customers ?

Thanks

Best Regards

Pier

0 Kudos
Reply
7,133 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Yes, you can share it.

0 Kudos
Reply
6,560 Views
gary_bisson
Senior Contributor III

Hi,

In that case, can you share that patch here directly?

Also, could you elaborate as to why this isn't in the tree in the first place?

Regards,
Gary

0 Kudos
Reply
7,101 Views
pierluigi_p
Senior Contributor I

Hi @Zhiming_Liu ,

can this approach be used for NANO too ?

Thanks

Best Regards

Pier

0 Kudos
Reply