i.MX8M Nano - SAI sync with another SAI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Nano - SAI sync with another SAI

ソリューションへジャンプ
2,052件の閲覧回数
pdgleonec
Contributor I

Hello,

I'm using the i.MX8M Nano to implement an audio system. I'm trying to confirm (or refute) that the SAI can synchronize with another SAI, in order to ensure if this would require hardware modifications or not.

On the one hand, this features seems documented, with the reserve that:

Synchronous operation between multiple SAI peripherals is not supported on all devices.

On the other hand, some elements seem to show that it is not supported:

1. A previous thread (here: https://community.nxp.com/t5/i-MX-Processors/iMX8-SAI3-and-SAI5-synchronous/td-p/1239416) indicates that the feature is not supported on i.MX8M Mini, which is close to the i.MX8M Nano.

2. The `fsl_sai` driver seems to not implement this feature (fsl_sai.h, l.116):

 

#define FSL_SAI_CR2_SYNC	BIT(30)

 

This shows that the 31th bit, used to synchronize with another SAI, is not implemented.

Is our interpretation correct that synchronization between multiple SAI is not supported on the i.MX8M Nano ?

Thanks for your support.

Regards

ラベル(3)
タグ(2)
1 解決策
2,033件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Philip 

 

>Is our interpretation correct that synchronization between multiple SAI is not supported on the i.MX8M Nano ?

 

yes it is correct, except sai2&sai3 modules which have such synchronization as described below

and in sect.3.2. Two-Lane I2S interface   AN12667 i.MX 8M Mini to i.MX 8M Nano Design Compatibility Guide

 

1.jpg

 

Best regards
igor

元の投稿で解決策を見る

2 返答(返信)
2,034件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Philip 

 

>Is our interpretation correct that synchronization between multiple SAI is not supported on the i.MX8M Nano ?

 

yes it is correct, except sai2&sai3 modules which have such synchronization as described below

and in sect.3.2. Two-Lane I2S interface   AN12667 i.MX 8M Mini to i.MX 8M Nano Design Compatibility Guide

 

1.jpg

 

Best regards
igor

2,008件の閲覧回数
pdgleonec
Contributor I

Thanks for your answer, I hadn't seen that part.

0 件の賞賛
返信