i.MX8M Mini programming issue (After change eMMC)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini programming issue (After change eMMC)

ソリューションへジャンプ
1,245件の閲覧回数
Ben4
Contributor II

Hi,

We using imx-6.6 for our hardware board.

In first stage all going well without any issue (eMMC is SDINBDG4 series)

And now we want to change to more larger size eMMC with SDINBDA6 series

, so we do some rework on current hardware board and just only change eMMC IC

But now, we could not programming firmware successfully with below error log,

 

Log Start

Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for mfgtools
, using default environment

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0

## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
Failed to configure default pinctrl
Detect USB boot. Will enter fastboot mode!
flash target is MMC:1
Card did not respond to voltage select! : -110
MMC card init failed!
Card did not respond to voltage select! : -110
** Block device MMC 1 not supported
Detect USB boot. Will enter fastboot mode!
flash target is MMC:2
MMC card init failed!
** Block device MMC 2 not supported

 

 

Would it be possible for me to kindly ask for some of your advice?

I truly appreciate it~ Thank you so much.

 

 

 

0 件の賞賛
返信
1 解決策
1,203件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Ben4 

I hope you are doing very well.

 

Please refer to this community thread:

https://community.nxp.com/t5/i-MX-Processors/Error-flashing-emmc-on-imx6ull-EVK/td-p/1867286

It could be a voltage incompatibility issue.

 

Best regards,

Salas.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,204件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Ben4 

I hope you are doing very well.

 

Please refer to this community thread:

https://community.nxp.com/t5/i-MX-Processors/Error-flashing-emmc-on-imx6ull-EVK/td-p/1867286

It could be a voltage incompatibility issue.

 

Best regards,

Salas.

0 件の賞賛
返信
1,122件の閲覧回数
Ben4
Contributor II
Thank you very much.
After follow your information and rework more boards then we think there has no issue on this topics.
Thanks~