i.MX7ULP camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,980件の閲覧回数
m_c
Senior Contributor I

1. In i.MX Linux release note for L4.14.78, it said i.MX7ULP board support MIPI Camera CSI.

pastedImage_1.png

2. In i.MX7ULP EVK fact sheet and quick start guide, it didn't show camera interface.

3. In i.MX7ULP fact sheet, it said camera is parallel interface.

pastedImage_4.png

Which one is right?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,733件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello m.c,

The i.MX7ULP is currently in preproduction status so I would need to ask you to please contact your Distributor or FAE for technical inquiries for this processor.

Mi apologies for the inconvenience,
Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,733件の閲覧回数
terry_lv
NXP Employee
NXP Employee

Hi,

  There's only a VIU parallel interface for camera. But currently there's no i.MX VIU driver released (maybe because there's no VIU interface on EVK board).

  If customer need to connect a camera using VIU, please describe your camera here (interface, format, etc.).

  We've an unofficial VIU driver and maybe we can provide you for reference.

  Thanks!

Regards

Terry

0 件の賞賛
返信
2,733件の閲覧回数
ankitr_patel
Senior Contributor II

Hi m.c,

Adding to the above reply,

iMX7ULP has VIU (Video Interface Unit) that can capture camera images using parallel interface. Currently, the driver for VIU interface is under development. Still you can use existing fsl-viu.c as reference.

Regards,

Ankit Patel

2,734件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello m.c,

The i.MX7ULP is currently in preproduction status so I would need to ask you to please contact your Distributor or FAE for technical inquiries for this processor.

Mi apologies for the inconvenience,
Regards,

0 件の賞賛
返信