i.MX7ULP camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7ULP camera

Jump to solution
2,982 Views
m_c
Senior Contributor I

1. In i.MX Linux release note for L4.14.78, it said i.MX7ULP board support MIPI Camera CSI.

pastedImage_1.png

2. In i.MX7ULP EVK fact sheet and quick start guide, it didn't show camera interface.

3. In i.MX7ULP fact sheet, it said camera is parallel interface.

pastedImage_4.png

Which one is right?

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
2,735 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello m.c,

The i.MX7ULP is currently in preproduction status so I would need to ask you to please contact your Distributor or FAE for technical inquiries for this processor.

Mi apologies for the inconvenience,
Regards,

View solution in original post

0 Kudos
Reply
3 Replies
2,735 Views
terry_lv
NXP Employee
NXP Employee

Hi,

  There's only a VIU parallel interface for camera. But currently there's no i.MX VIU driver released (maybe because there's no VIU interface on EVK board).

  If customer need to connect a camera using VIU, please describe your camera here (interface, format, etc.).

  We've an unofficial VIU driver and maybe we can provide you for reference.

  Thanks!

Regards

Terry

0 Kudos
Reply
2,735 Views
ankitr_patel
Senior Contributor II

Hi m.c,

Adding to the above reply,

iMX7ULP has VIU (Video Interface Unit) that can capture camera images using parallel interface. Currently, the driver for VIU interface is under development. Still you can use existing fsl-viu.c as reference.

Regards,

Ankit Patel

2,736 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello m.c,

The i.MX7ULP is currently in preproduction status so I would need to ask you to please contact your Distributor or FAE for technical inquiries for this processor.

Mi apologies for the inconvenience,
Regards,

0 Kudos
Reply