i.MX7D device tree configuration for ethernet DP83825

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX7D device tree configuration for ethernet DP83825

跳至解决方案
3,324 次查看
Ahmet_Cihan_AKINCA
Contributor III

Hi,

I'm currently integrating the DP83825 Ethernet IC with my i.MX7DSABRESD system. Previously, the board functioned perfectly with the RTL8211 IC. Due to supply chain disruptions, we opted to switch Ethernet ICs. However, I've encountered difficulties getting the DP83825 to work despite my troubleshooting efforts.

Kernel version is; Linux imx7dsabresd 5.4.70-2.3.11+gb34a9c9644c1 

Related part of my device tree;

 

&fec1 {
     pinctrl-names = "default";
     pinctrl-0 = <&pinctrl_enet1>;
    
     clocks = <&clks IMX7D_ENET_AXI_ROOT_CLK>,
         <&clks IMX7D_ENET_AXI_ROOT_CLK>,
         <&clks IMX7D_ENET1_TIME_ROOT_CLK>,
         <&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
         <&clks IMX7D_ENET1_REF_ROOT_DIV>;
    
     clock-names = "ipg", "ahb", "ptp", "enet_clk_ref","enet_out";
     assigned-clocks = <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
        	 <&clks IMX7D_ENET1_TIME_ROOT_CLK>;
     assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
     assigned-clock-rates = <0>, <100000000>;
     phy-mode = "rmii";
     phy-handle = <&ethphy0>;
     fsl,magic-packet;
     status = "okay";
    
    mdio {
        #address-cells = <1>;
        #size-cells = <0>;

        ethphy0: ethernet-phy@0 {
		 compatible = "ethernet-phy-ieee802.3-c22";
  		 reg = <0>;
        };
    };
};

&iomuxc {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_hog>;

    imx7d-sdb {
	        pinctrl_enet1: enet1grp {
     	   fsl,pins = <
     		   MX7D_PAD_GPIO1_IO10__ENET1_MDIO 		   0x3
     		   MX7D_PAD_GPIO1_IO11__ENET1_MDC 		   0x3
     		   
     		   MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0    0x1
     		   MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1    0x1
     		   
     		   MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL    0x1
     		   
     		   MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER    0x1
     		   
     		   MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0    0x1
     		   MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1    0x1

     		   MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL    0x1
     		   MX7D_PAD_ENET1_TX_CLK__CCM_ENET_REF_CLK1 0x40000001
     	   >;
        };
….

 

 Pin connections are as this;

Screenshot from 2024-04-05 17-26-51.png

Dmesg output is;

[ 1.243155] fec 30be0000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 1.249973] fec 30be0000.ethernet: Using random MAC address: 56:47:52:60:e4:f0
[ 1.258273] libphy: fec_enet_mii_bus: probed
[ 1.264233] fec 30be0000.ethernet eth0: registered PHC device 0
[ 8.445135] Generic PHY 30be0000.ethernet-1:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=30be0000.ethernet-1:00, irq=POLL)

 ifconfig and ethtool outputs

Ahmet_Cihan_AKINCA_1-1712327486248.png

Ahmet_Cihan_AKINCA_2-1712327511954.png

Since the speed and duplex settings are currently unknown, it suggests there might be a problem with the driver.

I can see MDIO and MDCLK at 2.5 MHz, and ETH_REF Clock at 50 MHz with an oscilloscope. However, there's no activity on TXD[0,1], RXD[0,1], TX_EN, RX_CTL, or RXC pins. All of these pins are low.

Do you have any suggestions on how to troubleshoot this issue?

0 项奖励
回复
1 解答
3,038 次查看
Ahmet_Cihan_AKINCA
Contributor III

I finally resolved the problem. It turned out to be a hardware problem. I had to connect the reference clock to GPIO1_12 to fix it. Let me show you the specific changes I made – perhaps they might be helpful for others working with RMII..

Here are the changes I made in u-boot;

in include/configs/mx7dsabresd.h file

 

#define CONFIG_FEC_XCV_TYPE RMII

 

in board/freescale/mx7dsabresd/mx7dsabresd.c file

 

static iomux_v3_cfg_t const fec1_pads[] = {
	MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_GPIO1_IO12__CCM_ENET_REF_CLK1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_GPIO1_IO10__ENET1_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL_MII),
	MX7D_PAD_GPIO1_IO11__ENET1_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL_MII),
};
...
static int setup_fec(void)
{
	struct iomuxc_gpr_base_regs *const iomuxc_gpr_regs
		= (struct iomuxc_gpr_base_regs *) IOMUXC_GPR_BASE_ADDR;
	int ret;

	clrsetbits_le32(&iomuxc_gpr_regs->gpr[1],
		(IOMUXC_GPR_GPR1_GPR_ENET1_TX_CLK_SEL_MASK |
		 IOMUXC_GPR_GPR1_GPR_ENET1_CLK_DIR_MASK), 0);

	ret = set_clk_enet(ENET_50MHz);
	if (ret)
		return ret;
	return 0;
}
int board_phy_config(struct phy_device *phydev)
{
	phy_write(phydev, MDIO_DEVAD_NONE, 0x1f, 0x4000);	//software reset
	if (phydev->drv->config)
		phydev->drv->config(phydev);
	return 0;
}

 

After these change, in u-boot we can see "alive" message for a ping;

Ahmet_Cihan_AKINCA_0-1714042822060.png

Here are the changes I made in kernel;

in /tmp/work-shared/imx7dsabresd/kernel-source/arch/arm/boot/dts/imx7d-sdb.dts file;

 

&fec1 {
	 pinctrl-names = "default";
	 pinctrl-0 = <&pinctrl_enet1>;
	 
	 clocks = <&clks IMX7D_ENET_AXI_ROOT_CLK>,
	 	<&clks IMX7D_ENET_AXI_ROOT_CLK>,
	 	<&clks IMX7D_ENET1_TIME_ROOT_CLK>,
	 	<&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
	 	<&clks IMX7D_ENET1_REF_ROOT_DIV>;
	 
	 clock-names = "ipg", "ahb", "ptp", "enet_clk_ref","no_enet_out";
	 assigned-clocks = <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
	 		<&clks IMX7D_ENET1_TIME_ROOT_CLK>;
	 assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
	 assigned-clock-rates = <0>, <100000000>;
	 phy-mode = "rmii";
	 phy-handle = <&ethphy0>;
	 fsl,magic-packet;
	 status = "okay";

	mdio {
  	  #address-cells = <1>;
  	  #size-cells = <0>;

  	  ethphy0: ethernet-phy@0 {
 		compatible = "ethernet-phy-ieee802.3-c22";
   		reg = <0>;
  	  };
	};
};
...
pinctrl_enet1: enet1grp {
  fsl,pins = <
  	MX7D_PAD_GPIO1_IO10__ENET1_MDIO  		  0x3
  	MX7D_PAD_GPIO1_IO11__ENET1_MDC  		  0x3
  	MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0	  0x1
  	MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1	  0x1
        MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL	  0x1
  	MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER	          0x1
  	MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0	  0x1
  	MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1	  0x1
        MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL	  0x1
  	MX7D_PAD_GPIO1_IO12__CCM_ENET_REF_CLK1  	  0x1  
  >;
};

 

In addition, I had to modify some code related to GPIO_1_12 because other peripherals, such as SPI4, were already using this pin.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,039 次查看
Ahmet_Cihan_AKINCA
Contributor III

I finally resolved the problem. It turned out to be a hardware problem. I had to connect the reference clock to GPIO1_12 to fix it. Let me show you the specific changes I made – perhaps they might be helpful for others working with RMII..

Here are the changes I made in u-boot;

in include/configs/mx7dsabresd.h file

 

#define CONFIG_FEC_XCV_TYPE RMII

 

in board/freescale/mx7dsabresd/mx7dsabresd.c file

 

static iomux_v3_cfg_t const fec1_pads[] = {
	MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1 | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER | MUX_PAD_CTRL(ENET_RX_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_GPIO1_IO12__CCM_ENET_REF_CLK1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
	MX7D_PAD_GPIO1_IO10__ENET1_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL_MII),
	MX7D_PAD_GPIO1_IO11__ENET1_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL_MII),
};
...
static int setup_fec(void)
{
	struct iomuxc_gpr_base_regs *const iomuxc_gpr_regs
		= (struct iomuxc_gpr_base_regs *) IOMUXC_GPR_BASE_ADDR;
	int ret;

	clrsetbits_le32(&iomuxc_gpr_regs->gpr[1],
		(IOMUXC_GPR_GPR1_GPR_ENET1_TX_CLK_SEL_MASK |
		 IOMUXC_GPR_GPR1_GPR_ENET1_CLK_DIR_MASK), 0);

	ret = set_clk_enet(ENET_50MHz);
	if (ret)
		return ret;
	return 0;
}
int board_phy_config(struct phy_device *phydev)
{
	phy_write(phydev, MDIO_DEVAD_NONE, 0x1f, 0x4000);	//software reset
	if (phydev->drv->config)
		phydev->drv->config(phydev);
	return 0;
}

 

After these change, in u-boot we can see "alive" message for a ping;

Ahmet_Cihan_AKINCA_0-1714042822060.png

Here are the changes I made in kernel;

in /tmp/work-shared/imx7dsabresd/kernel-source/arch/arm/boot/dts/imx7d-sdb.dts file;

 

&fec1 {
	 pinctrl-names = "default";
	 pinctrl-0 = <&pinctrl_enet1>;
	 
	 clocks = <&clks IMX7D_ENET_AXI_ROOT_CLK>,
	 	<&clks IMX7D_ENET_AXI_ROOT_CLK>,
	 	<&clks IMX7D_ENET1_TIME_ROOT_CLK>,
	 	<&clks IMX7D_PLL_ENET_MAIN_50M_CLK>,
	 	<&clks IMX7D_ENET1_REF_ROOT_DIV>;
	 
	 clock-names = "ipg", "ahb", "ptp", "enet_clk_ref","no_enet_out";
	 assigned-clocks = <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
	 		<&clks IMX7D_ENET1_TIME_ROOT_CLK>;
	 assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
	 assigned-clock-rates = <0>, <100000000>;
	 phy-mode = "rmii";
	 phy-handle = <&ethphy0>;
	 fsl,magic-packet;
	 status = "okay";

	mdio {
  	  #address-cells = <1>;
  	  #size-cells = <0>;

  	  ethphy0: ethernet-phy@0 {
 		compatible = "ethernet-phy-ieee802.3-c22";
   		reg = <0>;
  	  };
	};
};
...
pinctrl_enet1: enet1grp {
  fsl,pins = <
  	MX7D_PAD_GPIO1_IO10__ENET1_MDIO  		  0x3
  	MX7D_PAD_GPIO1_IO11__ENET1_MDC  		  0x3
  	MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0	  0x1
  	MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1	  0x1
        MX7D_PAD_ENET1_RGMII_TX_CTL__ENET1_RGMII_TX_CTL	  0x1
  	MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER	          0x1
  	MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0	  0x1
  	MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1	  0x1
        MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL	  0x1
  	MX7D_PAD_GPIO1_IO12__CCM_ENET_REF_CLK1  	  0x1  
  >;
};

 

In addition, I had to modify some code related to GPIO_1_12 because other peripherals, such as SPI4, were already using this pin.

0 项奖励
回复
3,254 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Is there any logs of link is not ready missing?

There probably is not a link set between MAC and PHY, could you provide the dump for mdio in u-boot to confirm this?

Is this issue persistent in u-boot? Can you ping in u-boot?

Regards

0 项奖励
回复
3,244 次查看
Ahmet_Cihan_AKINCA
Contributor III

Thank you for your reply Josephlinares.

My u-boot version is;

Screenshot from 2024-04-13 17-09-41.png

I set ip address 192.168.1.177

when I ping, I get this;

Screenshot from 2024-04-13 17-11-59.png

After writing

 

mdio write 0x1F 0x4000

 

which is software reset. I get this message in kernel space;

Screenshot from 2024-04-13 17-17-54.pngand "ethtool eth0" shows me
Speed: 100 MB/s

Duplex: Full

Screenshot from 2024-04-13 17-38-48.png

If I don't write "mdio write 0x1F 0x4000" on u-boot I see

Speed: Unknown!
Duplex: Unknown!
link detected : no

here. In u-boot, I have changed #define CONFIG_FEC_XCV_TYPE         RGMII

to RMII in ./include/configs/mx7dsabresd.h .

Also, in  ./board/freescale/mx7dsabresd/mx7dsabresd.c  I have changed

ret = set_clk_enet(ENET_125MHz)

to ENET_50MHZ

Still I cannot get ping ..

0 项奖励
回复
3,194 次查看
opedis
Contributor III

The question is from the phy not the i.MX. 

You need to ask phy vendor TI for phy fixup or check the linux source code if there is existing phy fixup for DP83825. 

If just "mdio write 0x1F 0x4000", you can write down the phy fixup. 

 

phy_register_fixup_for_uid(PHY_ID_DP83825, DP83825_PHY_ID_MASK,
dp83825_phy_fixup)

0 项奖励
回复
3,185 次查看
opedis
Contributor III

 

I checked the device tree, TI has binding guide for 83822, but it should be the same for  83825

https://www.kernel.org/doc/Documentation/devicetree/bindings/net/ti%2Cdp83822.yamlhttps://www.kernel...

  ti,rmii-mode:
    description: |
       If present, select the RMII operation mode. Two modes are
       available:
         - RMII master, where the PHY outputs a 50MHz reference clock which can
         be connected to the MAC.
         - RMII slave, where the PHY expects a 50MHz reference clock input
         shared with the MAC.
       The RMII operation mode can also be configured by its straps.
       If the strap pin is not set correctly or not set at all, then this can be
       used to configure it.
    $ref: /schemas/types.yaml#/definitions/string
    enum:
      - master
      - slave

required:

 

0 项奖励
回复
3,119 次查看
Ahmet_Cihan_AKINCA
Contributor III

Thank you for your help opedis. I appreciate your suggestion (phy_register_fixup_for_uid). I think, I have to try it work in u-boot first. u-boot is less complicated than kernel.

0 项奖励
回复