i.MX7D based Custom Board with LPDDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7D based Custom Board with LPDDR2

Jump to solution
1,637 Views
Wolf4
Contributor I

we are working on an i.MX7D based Custom Board with LPDDR2 Memory

(PoP Package soldered on PCB)

Organisation:  4Gb, 128Mx32 , 1xDie, 1xRank, 1xChannel, 533 MHz

The design is now already in the layout state.

Is there any Script aid  or other information out to program the memory parameters?

Thanx

Labels (1)
0 Kudos
Reply
1 Solution
1,531 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wolf4

please create service request for providing more help.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,532 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wolf4

please create service request for providing more help.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply