iMX6SX ENET1_RGMII_TXC Description

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6SX ENET1_RGMII_TXC Description

ソリューションへジャンプ
1,580件の閲覧回数
vadimaleynikov
Contributor III

Hi,

The IMX6SXRM descibes the ENET1_RGMII_TXC signal as "Serial output Ethernet data. Only valid during TX_EN assertion." in Table 24-1. What is the correct description of the ENET1_RGMII_TXC signal?

Best regards,
Vadim Aleynikov

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,432件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

this is clock which is clocking rgmii data, depicted on

Figure 54. RGMII Transmit Signal Timing Diagram Original i.MX6SX Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SXCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,433件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

this is clock which is clocking rgmii data, depicted on

Figure 54. RGMII Transmit Signal Timing Diagram Original i.MX6SX Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SXCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信