i.MX7 PXP and Bayer RGB data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX7 PXP and Bayer RGB data

跳至解决方案
2,251 次查看
fabian1993
Contributor I

Hello

In the reference manual I have read the following about the csi interface:

"Bayer data is a type of raw data from the image sensor. This byte-wide data must be
converted to the RGB space or YUV space by software. The data path for Bayer data is
from the CSI to memory". 

So the csi interface can't demosaic the bayer rgb data. What about the pixel pipeline, can it convert the data

to rgb?

Thank you

标签 (2)
0 项奖励
回复
1 解答
1,857 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

supported PxP CSC formats are described in sect.13.7.3 Top-level architecture i.MX7D Reference Manual,

I am afraid raw data convertion to rgb is not supported.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,858 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

supported PxP CSC formats are described in sect.13.7.3 Top-level architecture i.MX7D Reference Manual,

I am afraid raw data convertion to rgb is not supported.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复