i.MX7 PXP and Bayer RGB data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7 PXP and Bayer RGB data

ソリューションへジャンプ
2,252件の閲覧回数
fabian1993
Contributor I

Hello

In the reference manual I have read the following about the csi interface:

"Bayer data is a type of raw data from the image sensor. This byte-wide data must be
converted to the RGB space or YUV space by software. The data path for Bayer data is
from the CSI to memory". 

So the csi interface can't demosaic the bayer rgb data. What about the pixel pipeline, can it convert the data

to rgb?

Thank you

ラベル(2)
0 件の賞賛
返信
1 解決策
1,858件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

supported PxP CSC formats are described in sect.13.7.3 Top-level architecture i.MX7D Reference Manual,

I am afraid raw data convertion to rgb is not supported.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,859件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

supported PxP CSC formats are described in sect.13.7.3 Top-level architecture i.MX7D Reference Manual,

I am afraid raw data convertion to rgb is not supported.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信