USB supplied while i.MX6 is off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB supplied while i.MX6 is off

Jump to solution
3,149 Views
electricar
Contributor I

Hello,

am I getting this right, that it's not a problem when the USB ports of the i.MX6 are powered from another device while the i.MX6 is off (not powered)?

Thank you very much in advance.

Kind regards

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,072 Views
igorpadykov
NXP Employee
NXP Employee

Hi

you are right, i.MX6DQ Datasheet sect.4.2.1 Power-Up Sequence describes:

USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and can be powered at any time.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,073 Views
igorpadykov
NXP Employee
NXP Employee

Hi

you are right, i.MX6DQ Datasheet sect.4.2.1 Power-Up Sequence describes:

USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and can be powered at any time.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply