i.MX7 PXP and Bayer RGB data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 PXP and Bayer RGB data

Jump to solution
2,245 Views
fabian1993
Contributor I

Hello

In the reference manual I have read the following about the csi interface:

"Bayer data is a type of raw data from the image sensor. This byte-wide data must be
converted to the RGB space or YUV space by software. The data path for Bayer data is
from the CSI to memory". 

So the csi interface can't demosaic the bayer rgb data. What about the pixel pipeline, can it convert the data

to rgb?

Thank you

Labels (2)
0 Kudos
Reply
1 Solution
1,851 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

supported PxP CSC formats are described in sect.13.7.3 Top-level architecture i.MX7D Reference Manual,

I am afraid raw data convertion to rgb is not supported.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,852 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

supported PxP CSC formats are described in sect.13.7.3 Top-level architecture i.MX7D Reference Manual,

I am afraid raw data convertion to rgb is not supported.

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply