i.MX6UL EVK kernel debugging with ARM DSTREAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL EVK kernel debugging with ARM DSTREAM

1,677 次查看
muhammadbilal
Contributor I

HI,

I'm trying to debug kernel debug using DSTREAM on
i.mx6ul-evk board but DSTREAM does not connect with linux kernel.


Although I can easily connect and debug the bare metal and u-boot
application on this board.

My linux kernel distribution is based on yocto 4.1.37 version.
I am using RCF file from DS-5 installtion directory
/DS-5_v5.26.0/sw/debugger/configdb/Boards/NXP/i.MX6 UltraLite
(Generic)/i.MX6 UltraLite (Generic).rcf

I have also read AN5229.pdf about kernel debugging but not found
001-For-DS-5-debug-and-uart-console-work-normally.patch any where

How can I debug linux kernel on imx6ul-evk board using DSTREAM?

Thanks,
-Bilal

标签 (1)
0 项奖励
回复
1 回复

1,447 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Bilal

please find attached patch, also may be useful to

apply to vendor of DS5 (www.arm.com) directly for help with linux.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复