Enable and Distribute IRQs in Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable and Distribute IRQs in Linux

3,162件の閲覧回数
saravanankrish
Contributor I

Hello,

I am using imx6 sabrelite board in which Linux OS runs on core0 and RTOS on core1. I have configured GIC interrupt registers in RTOS but Linux OS overwrites it. I need to enable IRQs 88,142,143,150 and distribute it to core 1(RTOS) in linux source code. I have gone through the irq_gic.c file but couldn't get an idea to proceed further.

i have tried cat /proc/interrupts in serial console and i couldn't see the above IRQ numbers. is that indicates the above interrupts are disabled in Linux?

How to enable and distribute interrupts in Linux source code?

Your suggestions are welcome!

Thanks in advance.

0 件の賞賛
返信
1 返信

2,978件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi saravan

please refer to generic linux documentation on found on web, like

Linux Device Drivers, 2nd Edition: Chapter 9: Interrupt Handling 

4.6. Interrupt Handling - Understanding the Linux Kernel, 3rd Edition [Book] 

and sect.3.2 Interrupts (Operation) attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信