i.MX6SL: uSDHC Boot eFuse Descriptions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SL: uSDHC Boot eFuse Descriptions

Jump to solution
1,837 Views
norishinozaki
Contributor V

Hello Champs,

In the RM ver2, BOOT_CFG2[1] looks to be allocated only for SD2.

This is a typo and actually true to all of 4 uSDHC ports, right?

pastedImage_0.png

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
1 Solution
1,770 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

Table 5-4. SD/eSD Boot Fusemap  RM (address 0x470[7:0])

provides other uSDHC ports selection through fuses. GPIO option

only for SD2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,771 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

Table 5-4. SD/eSD Boot Fusemap  RM (address 0x470[7:0])

provides other uSDHC ports selection through fuses. GPIO option

only for SD2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,770 Views
norishinozaki
Contributor V

Hi Igor,

Thank you!

Nori Shinozaki

0 Kudos
Reply