i.MX6SL: uSDHC Boot eFuse Descriptions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SL: uSDHC Boot eFuse Descriptions

ソリューションへジャンプ
1,844件の閲覧回数
norishinozaki
Contributor V

Hello Champs,

In the RM ver2, BOOT_CFG2[1] looks to be allocated only for SD2.

This is a typo and actually true to all of 4 uSDHC ports, right?

pastedImage_0.png

Best regards,

Nori Shinozaki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,777件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

Table 5-4. SD/eSD Boot Fusemap  RM (address 0x470[7:0])

provides other uSDHC ports selection through fuses. GPIO option

only for SD2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,778件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

Table 5-4. SD/eSD Boot Fusemap  RM (address 0x470[7:0])

provides other uSDHC ports selection through fuses. GPIO option

only for SD2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,777件の閲覧回数
norishinozaki
Contributor V

Hi Igor,

Thank you!

Nori Shinozaki

0 件の賞賛
返信