i.MX6SDL GC320 performance.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6SDL GC320 performance.

跳至解决方案
2,416 次查看
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6SDL GPU.

We consider using GPU GC320 for overlay and resize, clipping.

Then, we want to know the GC320 performance.

According to the Vivante site, GC320 pixel rate is up to 1000M pixels/sec.

Composition Processsing Cores (CPC) | Vivante Corporation

So it is sufficient to do "1080p@30fps + 1080p@30fps overlay and 1080p@30fps -> SXGA (1280x1024)@30fps resizing" or "1080p@30fps + 1080p@30fps overlay and 1080p@30fps -> SXGA (1280x1024)@30fps clipping".

Is this correct?

Best Regards,

Satoshi Shimoda

标签 (3)
标记 (3)
0 项奖励
回复
1 解答
1,874 次查看
art
NXP Employee
NXP Employee

Yes, this is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,875 次查看
art
NXP Employee
NXP Employee

Yes, this is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复