i.MX6SDL GC320 performance.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SDL GC320 performance.

Jump to solution
2,418 Views
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6SDL GPU.

We consider using GPU GC320 for overlay and resize, clipping.

Then, we want to know the GC320 performance.

According to the Vivante site, GC320 pixel rate is up to 1000M pixels/sec.

Composition Processsing Cores (CPC) | Vivante Corporation

So it is sufficient to do "1080p@30fps + 1080p@30fps overlay and 1080p@30fps -> SXGA (1280x1024)@30fps resizing" or "1080p@30fps + 1080p@30fps overlay and 1080p@30fps -> SXGA (1280x1024)@30fps clipping".

Is this correct?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (3)
0 Kudos
Reply
1 Solution
1,876 Views
art
NXP Employee
NXP Employee

Yes, this is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,877 Views
art
NXP Employee
NXP Employee

Yes, this is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply