i.MX6SDL GC320 performance.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SDL GC320 performance.

ソリューションへジャンプ
2,452件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6SDL GPU.

We consider using GPU GC320 for overlay and resize, clipping.

Then, we want to know the GC320 performance.

According to the Vivante site, GC320 pixel rate is up to 1000M pixels/sec.

Composition Processsing Cores (CPC) | Vivante Corporation

So it is sufficient to do "1080p@30fps + 1080p@30fps overlay and 1080p@30fps -> SXGA (1280x1024)@30fps resizing" or "1080p@30fps + 1080p@30fps overlay and 1080p@30fps -> SXGA (1280x1024)@30fps clipping".

Is this correct?

Best Regards,

Satoshi Shimoda

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
1,910件の閲覧回数
art
NXP Employee
NXP Employee

Yes, this is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,911件の閲覧回数
art
NXP Employee
NXP Employee

Yes, this is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信