i.MX6S die temperature sensor accuracy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6S die temperature sensor accuracy

跳至解决方案
4,095 次查看
bipinbhatt
Contributor II

Hi All,

We are using i.MX6 Solo processor in project.

During thermal testing, we observed that our CPU is not able to boot at high temperature (Ta=65Degree) because i.MX6 internal temperature sensor is reading temperature that exceeds threshold point.

Does anybody know about accuracy of the CPU die temperature sensor?

Also the maximum tolerance of internal die temperature sensor and calibration of sensor.


Thanks in advance,

Bipin Bhatt

标签 (1)
0 项奖励
回复
1 解答
3,454 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Bipin

accuracy (variation of readings)  is ~10deg (+/-10deg).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,455 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Bipin

accuracy (variation of readings)  is ~10deg (+/-10deg).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,454 次查看
bipinbhatt
Contributor II

Hello Igor,

Thanks for your reply.

Does freescale documentation specify the accuracy of sensor anywhere?

Where did you find the above information?

Best regards,

Bipin

0 项奖励
回复
3,454 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Bipin

this is internal info.

Best regards

igor

0 项奖励
回复
3,454 次查看
bipinbhatt
Contributor II

OK.

Thank you.

Thanks & Regards,

Bipinchandra Bhatt

0 项奖励
回复