i.MX6S die temperature sensor accuracy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6S die temperature sensor accuracy

Jump to solution
2,075 Views
bipinbhatt
Contributor II

Hi All,

We are using i.MX6 Solo processor in project.

During thermal testing, we observed that our CPU is not able to boot at high temperature (Ta=65Degree) because i.MX6 internal temperature sensor is reading temperature that exceeds threshold point.

Does anybody know about accuracy of the CPU die temperature sensor?

Also the maximum tolerance of internal die temperature sensor and calibration of sensor.


Thanks in advance,

Bipin Bhatt

Labels (1)
0 Kudos
Reply
1 Solution
1,434 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bipin

accuracy (variation of readings)  is ~10deg (+/-10deg).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,435 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bipin

accuracy (variation of readings)  is ~10deg (+/-10deg).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,434 Views
bipinbhatt
Contributor II

Hello Igor,

Thanks for your reply.

Does freescale documentation specify the accuracy of sensor anywhere?

Where did you find the above information?

Best regards,

Bipin

0 Kudos
Reply
1,434 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bipin

this is internal info.

Best regards

igor

0 Kudos
Reply
1,434 Views
bipinbhatt
Contributor II

OK.

Thank you.

Thanks & Regards,

Bipinchandra Bhatt

0 Kudos
Reply