i.MX6Q multiple camera interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q multiple camera interface

Jump to solution
2,095 Views
chandrashekharv
Contributor II

Hi,

We have an requirement to connect 03 cameras to i.MX6Q processor, Will below hardware interface works to stream all three videos parallel.

1. Parallel interface --> 02 cameras

pastedImage_2.png

2. Mipi interface --> 01 camera.

pastedImage_1.png

Rgds

Chandra

Labels (1)
1 Solution
1,898 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chandra

this solution is feasible if there are no muxing pin conflicts, also may be useful to check

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,898 Views
chandrashekharv
Contributor II

Thanks Igor, We will make an hardware. Hope in latest available kernel all BSP changes available.

Rgds

Chandra

0 Kudos
Reply
1,899 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chandra

this solution is feasible if there are no muxing pin conflicts, also may be useful to check

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------