i.MX6Q multiple camera interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q multiple camera interface

ソリューションへジャンプ
2,208件の閲覧回数
chandrashekharv
Contributor II

Hi,

We have an requirement to connect 03 cameras to i.MX6Q processor, Will below hardware interface works to stream all three videos parallel.

1. Parallel interface --> 02 cameras

pastedImage_2.png

2. Mipi interface --> 01 camera.

pastedImage_1.png

Rgds

Chandra

ラベル(1)
1 解決策
2,011件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chandra

this solution is feasible if there are no muxing pin conflicts, also may be useful to check

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,011件の閲覧回数
chandrashekharv
Contributor II

Thanks Igor, We will make an hardware. Hope in latest available kernel all BSP changes available.

Rgds

Chandra

0 件の賞賛
返信
2,012件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chandra

this solution is feasible if there are no muxing pin conflicts, also may be useful to check

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------