Ragan_Dunham
		
			Ragan_Dunham
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I do not have any specific advice as souphttpsrc is not officially supported by Freescale. I am not certain what build environment you are using, but if you have not already I would check Yocto to see if there is support there (I did not check myself). If so, even if you are not using Yocto you could determine the other dependencies pretty quickly.
Best Regards,
Ragan
 
					
				
		
 Ragan_Dunham
		
			Ragan_Dunham
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I do not have any specific advice as souphttpsrc is not officially supported by Freescale. I am not certain what build environment you are using, but if you have not already I would check Yocto to see if there is support there (I did not check myself). If so, even if you are not using Yocto you could determine the other dependencies pretty quickly.
Best Regards,
Ragan
 
					
				
		
hi I am using imx6 BSP rootfs based L3.0.35_1.1.0_121218_source.
it support souphttpsrc!!!
you can test it as following ways:
1, udhcpc eth0; and gst-launch playbin2 uri=http://docs.gstreamer.com/media/sintel_trailer-480p.webm"
2,
a) use VLC to stream HTTP data. (mux=ts,without seekout),path:172.21.78.67:8080/1
b) at the end of imx6:
while true;do gst-launch souphttpsrc location=http://172.21.78.67:8080/1 ! mpegtsdemux name=ts ts. ! queue ! vpudec ! mfw_v4lsink sync=false ts. ! queue ! beepdec ! alsasink sync=false -vvv; done
thx
baihui ADV
 
					
				
		
Hi Tarek,
I think for that you also need to install libsoup as well. I think it is dependent upon it. I have not tried to install it though.
Tim
 
					
				
		
hi I am using imx6 BSP rootfs based L3.0.35_1.1.0_121218_source.
it support souphttpsrc!!!
you can test it as following ways:
1, udhcpc eth0; and gst-launch playbin2 uri=http://docs.gstreamer.com/media/sintel_trailer-480p.webm"
2,
a) use VLC to stream HTTP data. (mux=ts,without seekout),path:172.21.78.67:8080/1
b) at the end of imx6:
while true;do gst-launch souphttpsrc location=http://172.21.78.67:8080/1 ! mpegtsdemux name=ts ts. ! queue ! vpudec ! mfw_v4lsink sync=false ts. ! queue ! beepdec ! alsasink sync=false -vvv; done
thx
baihui ADV
 
					
				
		
Hi Tim,
I have installed libsoup then re-compiled gst-plugins-good. Still no luck thought :smileysad:
Tarek