I do not have any specific advice as souphttpsrc is not officially supported by Freescale. I am not certain what build environment you are using, but if you have not already I would check Yocto to see if there is support there (I did not check myself). If so, even if you are not using Yocto you could determine the other dependencies pretty quickly.
Best Regards,
Ragan
I do not have any specific advice as souphttpsrc is not officially supported by Freescale. I am not certain what build environment you are using, but if you have not already I would check Yocto to see if there is support there (I did not check myself). If so, even if you are not using Yocto you could determine the other dependencies pretty quickly.
Best Regards,
Ragan
hi I am using imx6 BSP rootfs based L3.0.35_1.1.0_121218_source.
it support souphttpsrc!!!
you can test it as following ways:
1, udhcpc eth0; and gst-launch playbin2 uri=http://docs.gstreamer.com/media/sintel_trailer-480p.webm"
2,
a) use VLC to stream HTTP data. (mux=ts,without seekout),path:172.21.78.67:8080/1
b) at the end of imx6:
while true;do gst-launch souphttpsrc location=http://172.21.78.67:8080/1 ! mpegtsdemux name=ts ts. ! queue ! vpudec ! mfw_v4lsink sync=false ts. ! queue ! beepdec ! alsasink sync=false -vvv; done
thx
baihui ADV
hi I am using imx6 BSP rootfs based L3.0.35_1.1.0_121218_source.
it support souphttpsrc!!!
you can test it as following ways:
1, udhcpc eth0; and gst-launch playbin2 uri=http://docs.gstreamer.com/media/sintel_trailer-480p.webm"
2,
a) use VLC to stream HTTP data. (mux=ts,without seekout),path:172.21.78.67:8080/1
b) at the end of imx6:
while true;do gst-launch souphttpsrc location=http://172.21.78.67:8080/1 ! mpegtsdemux name=ts ts. ! queue ! vpudec ! mfw_v4lsink sync=false ts. ! queue ! beepdec ! alsasink sync=false -vvv; done
thx
baihui ADV