i.MX6Dual RTC_XTALI,RTC_XTALO pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Dual RTC_XTALI,RTC_XTALO pins

ソリューションへジャンプ
2,456件の閲覧回数
佐藤智幸
Contributor I

Dear community,

I have a question about i.MX6Dual.

When I do not use external RTCXTAL(32.768k), is the RTC_XTALI,RTCXTALO pin good as a float?

Thanks and Best Regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
2,211件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 佐藤智幸

you should always use RTCXTAL(32.768k) due to

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,212件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 佐藤智幸

you should always use RTCXTAL(32.768k) due to

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信