i.MX6DQ PoP package pin multiplexing.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6DQ PoP package pin multiplexing.

跳至解决方案
1,578 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ PoP package.

You know the ball mapping of i.MX6DQ PoP package is different from FCBGA package.

Then, how about pin multiplexing?

Are same sigmals are muxed?

(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

Best Regards,

Satoshi Shimoda

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,502 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

pin multiplexing for i.MX6DQ PoP package is the same

as for FCBGA package.

>Are same sigmals are muxed?

>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

yes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,503 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

pin multiplexing for i.MX6DQ PoP package is the same

as for FCBGA package.

>Are same sigmals are muxed?

>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

yes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复