i.MX6DQ PoP package pin multiplexing.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ PoP package pin multiplexing.

ソリューションへジャンプ
1,579件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ PoP package.

You know the ball mapping of i.MX6DQ PoP package is different from FCBGA package.

Then, how about pin multiplexing?

Are same sigmals are muxed?

(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

Best Regards,

Satoshi Shimoda

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,503件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

pin multiplexing for i.MX6DQ PoP package is the same

as for FCBGA package.

>Are same sigmals are muxed?

>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

yes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,504件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

pin multiplexing for i.MX6DQ PoP package is the same

as for FCBGA package.

>Are same sigmals are muxed?

>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

yes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信