i.MX6DQ PoP package pin multiplexing.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ PoP package pin multiplexing.

Jump to solution
494 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ PoP package.

You know the ball mapping of i.MX6DQ PoP package is different from FCBGA package.

Then, how about pin multiplexing?

Are same sigmals are muxed?

(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (2)
0 Kudos
1 Solution
418 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

pin multiplexing for i.MX6DQ PoP package is the same

as for FCBGA package.

>Are same sigmals are muxed?

>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

yes.

Best regards

igor
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
419 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

pin multiplexing for i.MX6DQ PoP package is the same

as for FCBGA package.

>Are same sigmals are muxed?

>(e.g. for EIM_DA0 pad, muxed EIM_AD00, IPU1_DISP1_DATA09, GPIO3_IO00, and SRC_BOOT_CFG00 signals)

yes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos