i.MX6DL two pipelines playing for imxvideoconvert_g2d issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6DL two pipelines playing for imxvideoconvert_g2d issue

1,758 次查看
ganhongxing
Contributor I

env:

gstreamer-1.8.1

imx-gst1.0-plugin-4.1.1

qt-gstreamer

when playing two pipelines one time,

ex:  v4l2src device=/dev/video0 ! imxvideoconvert_g2d ratiton=0 !  qwidget5videosink

      v4l2src device=/dev/video1 ! imxvideoconvert_g2d ratiton=1 !  qwidget5videosink

two qt widget window

sometimes got errors: g2d_cache_op: fail with status -7g2d_cache_op: fail with status -7g2d_cache_op: fail with status -7g2d_open: fail with status -7

only one window has video.

how can i fix this ?

标签 (3)
0 项奖励
回复
4 回复数

1,532 次查看
1130692457
Contributor I

can you tell me how to install gstreamer in linux not through ubuntu

0 项奖励
回复

1,532 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you install any nxp bsp? like yocto? if yes, the bsp includes gstreamer already. what OS do you want to use?

0 项奖励
回复

1,532 次查看
1130692457
Contributor I

i want to uses the waf meta build system build my cross compilation ,But now I don't know how to change the environment variable, or how to compile and port the entire program to imx6.q,As you said, can yocto support gstreamer-imx?Thank you for your reply

0 项奖励
回复

1,532 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you play video to different outputu or  to the main window?

is this random error? how long will you get this error when you play the video?

0 项奖励
回复