i.MX6DL two pipelines playing for imxvideoconvert_g2d issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL two pipelines playing for imxvideoconvert_g2d issue

1,783 Views
ganhongxing
Contributor I

env:

gstreamer-1.8.1

imx-gst1.0-plugin-4.1.1

qt-gstreamer

when playing two pipelines one time,

ex:  v4l2src device=/dev/video0 ! imxvideoconvert_g2d ratiton=0 !  qwidget5videosink

      v4l2src device=/dev/video1 ! imxvideoconvert_g2d ratiton=1 !  qwidget5videosink

two qt widget window

sometimes got errors: g2d_cache_op: fail with status -7g2d_cache_op: fail with status -7g2d_cache_op: fail with status -7g2d_open: fail with status -7

only one window has video.

how can i fix this ?

Labels (3)
0 Kudos
Reply
4 Replies

1,557 Views
1130692457
Contributor I

can you tell me how to install gstreamer in linux not through ubuntu

0 Kudos
Reply

1,557 Views
joanxie
NXP TechSupport
NXP TechSupport

did you install any nxp bsp? like yocto? if yes, the bsp includes gstreamer already. what OS do you want to use?

0 Kudos
Reply

1,557 Views
1130692457
Contributor I

i want to uses the waf meta build system build my cross compilation ,But now I don't know how to change the environment variable, or how to compile and port the entire program to imx6.q,As you said, can yocto support gstreamer-imx?Thank you for your reply

0 Kudos
Reply

1,557 Views
joanxie
NXP TechSupport
NXP TechSupport

did you play video to different outputu or  to the main window?

is this random error? how long will you get this error when you play the video?

0 Kudos
Reply