i.MX6 without RTC XTAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 without RTC XTAL

Jump to solution
2,072 Views
JHY
Contributor IV

Can I use i.mx6 without RTC XTAL?

I have GPS module so RTC XTAL is not needed.

And how can I adjust time data from GPS module?

My system has linux 3.10.53.

Thank you.

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,784 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

without external crystal one can be affected by erratum

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,785 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

without external crystal one can be affected by erratum

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply