i.MX6 without RTC XTAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 without RTC XTAL

ソリューションへジャンプ
2,097件の閲覧回数
JHY
Contributor IV

Can I use i.mx6 without RTC XTAL?

I have GPS module so RTC XTAL is not needed.

And how can I adjust time data from GPS module?

My system has linux 3.10.53.

Thank you.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,809件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

without external crystal one can be affected by erratum

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,810件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

without external crystal one can be affected by erratum

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信