i.MX6 kernel boot parameter "ldb=" still active?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6 kernel boot parameter "ldb=" still active?

跳至解决方案
1,808 次查看
torus1000
Contributor V

All,

I remembered i.MX6 L3.0.35 supported dual LVDS display to set kernel parameter such as ldb=dul0.

Then I tried this for KK4.4.3 but some of them were ignored.

     c.f. u-boot=> setenv mmcargs .... ldb=dul0

           u-boot=> boot

The results were:
      ldb=dul1 OK                           #dual  (same output to 2 panels)
      ldb=sep  Fail(same as dul1)   #serarate
      ldb=spl1 Fail(same as dul1)   #split (2 ports for 1 panel)

Is this parameter still valid/alive?

Thanks.

标签 (3)
标记 (4)
0 项奖励
回复
1 解答
1,322 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Thorus,

Did this work for you with previous versions of android?.

As far as I know, android cannot send separate video through 2 different channels, that is why only dul1 works


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,323 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Thorus,

Did this work for you with previous versions of android?.

As far as I know, android cannot send separate video through 2 different channels, that is why only dul1 works


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,322 次查看
torus1000
Contributor V

Dear Sergio,

Thank you for your reply.

Have a nice day.

0 项奖励
回复