i.MX6 kernel boot parameter "ldb=" still active?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 kernel boot parameter "ldb=" still active?

ソリューションへジャンプ
1,816件の閲覧回数
torus1000
Contributor V

All,

I remembered i.MX6 L3.0.35 supported dual LVDS display to set kernel parameter such as ldb=dul0.

Then I tried this for KK4.4.3 but some of them were ignored.

     c.f. u-boot=> setenv mmcargs .... ldb=dul0

           u-boot=> boot

The results were:
      ldb=dul1 OK                           #dual  (same output to 2 panels)
      ldb=sep  Fail(same as dul1)   #serarate
      ldb=spl1 Fail(same as dul1)   #split (2 ports for 1 panel)

Is this parameter still valid/alive?

Thanks.

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 解決策
1,330件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Thorus,

Did this work for you with previous versions of android?.

As far as I know, android cannot send separate video through 2 different channels, that is why only dul1 works


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,331件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Thorus,

Did this work for you with previous versions of android?.

As far as I know, android cannot send separate video through 2 different channels, that is why only dul1 works


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,330件の閲覧回数
torus1000
Contributor V

Dear Sergio,

Thank you for your reply.

Have a nice day.

0 件の賞賛
返信