Hi,
We are using imx6Q custom platform based of sabresd platform and we are using Linux 3.10.17_1.0.0-GA BSP for our development.
We aware of below Errata in iMX6 Silicon.
ERR004512 ENET: 1 Gb Ethernet MAC (ENET) system limitation
The problem we are facing is, Ethernet interface degrading over the time.
Initially the Ethernet is working fine with 1000Mbps. But over a time, the Ethernet detects only 100Mbps if we connect with 1000Mbps network also.
Is there any errata describing this issue?
Please suggest us.
Regards,
Ansari
Please try using the recent Linux BSP (L3.10.53_1.1.0) for the i.MX6, which may be
found on the next Summary Page :
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW
Regards,
Yuri