i.MX6 ethernet smartbit test is failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 ethernet smartbit test is failed

1,031 次查看
charleshuang
Senior Contributor II

We did smartbit test on i.MX6 demo board, and found the problem happens at long length packet. Attached the complete test result.

Any suggestion for improving the test result.

 

 

Packet

Speed&

Packets

Bytes

Percent

Packets

Packets

Bytes

Bytes

Pct

Packets

Collisions

CRC

Alignment

Oversize

Undersize

Length

Duplex

/Second

/Second

Bandwidth

Sent

Received

Sent

Received

Received

Dropped

Errors

Errors

Errors

Errors

1020

GIG_FULL

11973

12260352

10

119730

119730

122603520

122603520

  1. 100.00
  2. 0.00

0

0

0

0

0

1020

GIG_FULL

23946

24520704

20

239460

126525

245207040

129561600

  1. 52.84
  2. 112935.00

0

0

0

0

0

1020

GIG_FULL

35919

36781056

30

359190

322634

367810560

330377216

  1. 89.82
  2. 36556.00

0

0

0

0

0

1020

GIG_FULL

47892

49041408

40

478920

283627

490414080

290434048

  1. 59.22
  2. 195293.00

0

0

0

0

0

1020

GIG_FULL

59865

61301760

50

598650

254216

613017600

260317184

  1. 42.46
  2. 344434.00

0

0

0

0

0

1020

GIG_FULL

71839

73563136

60

718390

239002

735631360

244738048

  1. 33.27
  2. 479388.00

0

0

0

0

0

1020

GIG_FULL

83836

85848064

70

838360

229989

858480640

235508736

  1. 27.43
  2. 608371.00

0

0

0

0

0

1020

GIG_FULL

95785

98083840

80

957850

225528

980838400

230940672

  1. 23.55
  2. 732322.00

0

0

0

0

0

1020

GIG_FULL

107758

110344192

90

1077580

232826

1103441920

238413824

  1. 21.61
  2. 844754.00

0

0

0

0

0

1020

GIG_FULL

119731

122604544

100

1197310

233618

1226045440

239224832

  1. 19.51
  2. 963692.00

0

0

0

0

0

1276

GIG_FULL

9615

12307200

10

96150

96150

123072000

123072000

  1. 100.00
  2. 0.00

0

0

0

0

0

1276

GIG_FULL

19230

24614400

20

192300

192288

246144000

246128640

  1. 99.99
  2. 12.00

0

0

0

0

0

1276

GIG_FULL

28848

36925440

30

288480

288477

369254400

369250560

  1. 100.00
  2. 3.00

0

0

0

0

0

1276

GIG_FULL

38461

49230080

40

384610

256042

492300800

327733760

  1. 66.57
  2. 128568.00

0

0

0

0

0

1276

GIG_FULL

48076

61537280

50

480760

213448

615372800

273213440

  1. 44.40
  2. 267312.00

0

0

0

0

0

1276

GIG_FULL

57710

73868800

60

577100

213929

738688000

273829120

  1. 37.07
  2. 363171.00

0

0

0

0

0

1276

GIG_FULL

67312

86159360

70

673120

202324

861593600

258974720

  1. 30.06
  2. 470796.00

0

0

0

0

0

1276

GIG_FULL

76923

98461440

80

769230

185972

984614400

238044160

  1. 24.18
  2. 583258.00

0

0

0

0

0

1276

GIG_FULL

86565

110803200

90

865650

189885

1108032000

243052800

  1. 21.94
  2. 675765.00

0

0

0

0

0

1276

GIG_FULL

96153

123075840

100

961530

195609

1230758400

250379520

  1. 20.34
  2. 765921.00

0

0

0

0

0

1514

GIG_FULL

8127

12336786

10

81270

81270

123367860

123367860

  1. 100.00
  2. 0.00

0

0

0

0

0

1514

GIG_FULL

16254

24673572

20

162540

127721

246735720

193880478

  1. 78.58
  2. 34819.00

0

0

0

0

0

1514

GIG_FULL

24385

37016430

30

243850

243385

370164300

369458430

  1. 99.81
  2. 465.00

0

0

0

0

0

1514

GIG_FULL

32509

49348662

40

325090

199818

493486620

303323724

  1. 61.47
  2. 125272.00

0

0

0

0

0

1514

GIG_FULL

40637

61686966

50

406370

182104

616869660

276433872

  1. 44.81
  2. 224266.00

0

0

0

0

0

1514

GIG_FULL

48770

74032860

60

487700

175060

740328600

265741080

  1. 35.90
  2. 312640.00

0

0

0

0

0

1514

GIG_FULL

56895

86366610

70

568950

158501

863666100

240604518

  1. 27.86
  2. 410449.00

0

0

0

0

0

1514

GIG_FULL

65036

98724648

80

650360

138244

987246480

209854392

  1. 21.26
  2. 512116.00

0

0

0

0

0

1514

GIG_FULL

73185

111094830

90

731850

134749

1110948300

204548982

  1. 18.41
  2. 597101.00

0

0

0

0

0

1514

GIG_FULL

81274

123373932

100

812740

159544

1233739320

242187792

  1. 19.63
  2. 653196.00

0

0

0

0

0

Original Attachment has been moved to: freescale_smartbits.rar

0 项奖励
回复
1 回复

867 次查看
charliechang
Contributor II

Dear Charles,

How to enable the i.mx6 can be tested by Smartbits?

Thank you.

0 项奖励
回复