i.MX6 encoding + decoding performance limit.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 encoding + decoding performance limit.

ソリューションへジャンプ
2,636件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 VPU capability.

I want to know the limit performance to encode and decode simltaneously.

According to page 7 of presentation in  Q&A: MX6 VPU H.264 Dual Stream Encode Limits , I think the following performances are limit.

[i.MX6SDL]

1080p@30fps decoding + 1080p@24fps encoding (since i.MX6SDL max VPU frequency is up to 328MHz < 350MHz)

720p@30fps 2streams decoding + 720p@24fps 2streams encoding (since i.MX6SDL max VPU frequency is up to 328MHz < 350MHz)

SD@30fps 4streamsd decoding + SD@30fps 4streams encoding

[i.MX6DQ]

1080p@30fps decoding + 1080p@30fps encoding

720p@30fps 2streams  decoding + 720p@30fps 2streams  encoding

SD@30fps 4streams  decoding + SD@30fps 4streams  encoding

Is my understanding correct?

Best Regards,

Satoshi Shimoda

ラベル(5)
タグ(1)
0 件の賞賛
返信
1 解決策
2,064件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think this performances understanding is right.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,065件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think this performances understanding is right.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信