Hello,
Strictly speaking, jitter or accuracy parameters of internal PLLs are not specified.
The only specified parameters may be found in the Datasheet(s) in section “PLL’s
Electrical Characteristics”. Nevertheless, we can refer to Table 1-14 (24 MHz crystal
tolerance guidelines) of the Hardware Development Guide, assuming stability (thermal,
voltage and other) of PLL output clock is fully defined by external crystal / oscillator,
and i.MX6 meets USB, PCIe, Ethernet clock specs.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------