i.MX6 and SyncE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,566件の閲覧回数
xav
Contributor II

Hi,

does i.MX6 SoloX allow to use SyncE ethernet ?

If not, does another i.MX chip allow it ? Or even the soon-to-be i.MX7 ?

Thanks,

        Xav

タグ(1)
0 件の賞賛
返信
1 解決策
2,455件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

unfortunately i.MX6SX, iMX7 do not support in

hardware SyncE. I am not aware of future chips

where it will be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,456件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

unfortunately i.MX6SX, iMX7 do not support in

hardware SyncE. I am not aware of future chips

where it will be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,455件の閲覧回数
xav
Contributor II

Hi Igor,

OK, I understand. Is it possible to still have SyncE by adding a different PHY, which will replace the built-in one ?

0 件の賞賛
返信
2,455件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xavier

I am afraid not, because except PHY, it should be also supported by i.MX MAC.

~igor

0 件の賞賛
返信
2,455件の閲覧回数
xav
Contributor II

I'm not so sure, this PHY DP83640 | PHY | Ethernet | Description & parametrics  has been used on a Sitara AM335x and make it support SyncE, which I don't think it does natively.

Would it be usable on an i.MX ?

0 件の賞賛
返信
2,455件の閲覧回数
xav
Contributor II

Would adding a dedicated PCIe ethernet chip work ?

0 件の賞賛
返信