Hello,
I'm wondering if there is a mistake or if I am misunderstanding what figure 64.2 in the i.MX6DQ RM states.
According to:
64.4.3.3 DTR_B: Input in DCE mode and output in DTE mode.
64.4.3.4 DSR_B: Output in DCE mode and input in DTE mode.
64.4.3.6 DCD_B: Output in DCE mode and input in DTE mode
64.4.3.7 RI_B: Output in DCE mode and input in DTE mode.
Ignoring the IOMUX function, figure 64.2 shows the exact opposite directions for these 4 signals in both DTE and DCE modes.
TX_DATA, RX_DATA, CTS_B and RTS_B behave as inputs or outputs, independent from DTE or DCE configurations, but the modem signals just don't match in this figure.
Am I getting a wrong interpretation here?
Thanks,
Guillermo
已解决! 转到解答。
Hi Guillermo
your interpretation is correct. In general recommended to use
Table 90. UART I/O Configuration vs. Mode IMX6DQCEC
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Guillermo
your interpretation is correct. In general recommended to use
Table 90. UART I/O Configuration vs. Mode IMX6DQCEC
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------