i.MX6 How to support SDXC function on Yocto 3.14.28_1.0.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 How to support SDXC function on Yocto 3.14.28_1.0.0?

1,876 Views
charleshuang
Senior Contributor II

Our current seems to support SDHC, so the maximal capacity of SD is only 32GB, but per this modification, we could support SDXC (SD 3.0), the maximal capacity of SD will be 2TB.

Please see attached file.

Question 1:  We want to support SDXC function. In addition to the hardware to be modified, does the software also need to modify?

If we need to modify software, how do we modify?

Question 2: If we do not modify the hardware and modify the above mentioned software aspects, will we have any problem happen?

Thank you.

Best Regards,

Alex Cheng

Labels (5)
0 Kudos
Reply
1 Reply

1,260 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alex

i.MX6 Sabre AI board supports sdxc on p.6 sch-27142

SABRE|Automotive-Infotainment|i.MX6|Freescale

as for software :

http://www.linuxquestions.org/questions/linux-hardware-18/what-about-sdxc-memory-cards-831839/

exfat-utils

Packages for Graphics, Multimedia, Networking, Development & more | Timesys Embedded Linux

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply