i.MX6/Enet: CRC/FCS errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6/Enet: CRC/FCS errors

ソリューションへジャンプ
2,145件の閲覧回数
bastian_schick
Contributor IV

Hi

I am noticed that I get FCS error while sending if TDAR is written even if it is set (100 out of 100,000 packets).

But this seems not to be the known erratum for the ENET.

I am using a i.MX6Q on a Phytec phyFlex-i.MX6Q board running non-linux, sending and receiving every 40us a packet.

I know there is a bandwidth limit (measured 600MB/s) but the FCS errors come even at a bandwidth of 200MB/s.

Did anyone experience the same?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,889件の閲覧回数
bastian_schick
Contributor IV

For reference: The problem wasn't TDAR or the errata, but a wrong IOMUX setup for the DDR-RAM: CMOS instead to differential on some pins. This resulted in a bit error from time to time.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,890件の閲覧回数
bastian_schick
Contributor IV

For reference: The problem wasn't TDAR or the errata, but a wrong IOMUX setup for the DDR-RAM: CMOS instead to differential on some pins. This resulted in a bit error from time to time.

0 件の賞賛
返信