iMX280 : CLKGATE bit effect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX280 : CLKGATE bit effect

ソリューションへジャンプ
1,646件の閲覧回数
koichisakagami
Contributor II

Dear community,

We consider a  i.MX280 power consumption.
As we hope to reduce the i.MX280 power consumption,
we check the clock tree for unused modules.

If we will gate off the unused module clocks,
does the i.MX280 power consumption decrease ?


Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,538件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

yes, gating unused module clocks

will decrease i.MX28 power consumption.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,539件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi koichi

yes, gating unused module clocks

will decrease i.MX28 power consumption.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信