Hi,
looking at the reference manual for the i.MX28 (Figure 10-1. Logical Diagram of Clock Domains, Chapter 10 Clock Generation and Control (CLKCTRL), i.MX28 Applications Processor Reference Manual, Rev. 2, 08/2013) doesn't show the clock domain for the DC-DC.
So i created a little ASCII art accordingly to the diagramm in the RM:
https://gist.github.com/lategoodbye/e59dbe134f74e49c4b52
Is it correct?
Thanks Stefan
解決済! 解決策の投稿を見る。
Generally Your figure is correct. Note : there is no option of DC_HALFCLK in HW_POWER_MINPWR.
From section 11.2.1.2 (DC-DC Extended Battery Life Features) of the i.MX28 Reference Manual :
"DC-DC Switching Frequency—The standard DC-DC switching frequency is 1.5
MHz, which provides a good mix of efficiency and power output. The frequency can
be reduced to 750 KHz to reduce operating current in some light load situations
through DC_HALFCLK in HW_POWER_MINPWR. The DC-DC converter can
also be programmed to a frequency that is based on PLL using the SEL_PLLCLK
and FREQSEL fields in the HW_POWER_MISC register."
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Generally Your figure is correct. Note : there is no option of DC_HALFCLK in HW_POWER_MINPWR.
From section 11.2.1.2 (DC-DC Extended Battery Life Features) of the i.MX28 Reference Manual :
"DC-DC Switching Frequency—The standard DC-DC switching frequency is 1.5
MHz, which provides a good mix of efficiency and power output. The frequency can
be reduced to 750 KHz to reduce operating current in some light load situations
through DC_HALFCLK in HW_POWER_MINPWR. The DC-DC converter can
also be programmed to a frequency that is based on PLL using the SEL_PLLCLK
and FREQSEL fields in the HW_POWER_MISC register."
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Yuri