Hi,
i'm currently working on mainline Linux drivers (regulator and power switch) for the i.MX23/i.MX28 PMU. According to reference manual (i.MX28 chapter 11.11)
there are interrupts which share the same interrupt line:
The VDDA_BO_IRQ, VDDD_BO_IRQ, VDDIO_BO_IRQ, and BATT_BO_IRQ each
have their own interrupt line back to the interrupt collector.
However, the remaining five interrupts—VDD5V_GT_VDDIO_IRQ, DC_OK_IRQ,
VBUSVALID_IRQ, LINREG_OK_IRQ and PSWITCH_IRQ—all share a single
interrupt line. In this case, software must read the interrupt status
bits to discover which event caused the interrupt.
For devicetree binding i have the following question:
Are these interrupts (VDD5V_GT_VDDIO_IRQ, DC_OK_IRQ, VBUSVALID_IRQ, LINREG_OK_IRQ and PSWITCH_IRQ) are generated by the PMU as a whole or
is it only a logical grouping of separate units and the interrupts get muxed together?
Stefan
Discussion on mailing list:
'Question about shared interrupts in devicetree' - MARC