i:MX27 "request_irq" returns with error code -22

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i:MX27 "request_irq" returns with error code -22

2,042 次查看
aneesrehman
Contributor I

Hi,

I am trying to port  a device driver from Linux kernel version 2.6.22 to kernel version 3.14.15  for i:MX27 based platform.

I am stuck with a problem :smileysad: the "request_irq" for gpio irq controller (irq number 24 in 3.14) returns an invalid value error

code. Although the call to request_irq returns successful when called for other gpio irq number such as irq 228.

Here is the code snippet:

"The device tree node where irq is  configured"

gpio_irq_hack {

compatible = "atlas,gpio_irq_hack";

interrupt-parent = <&aitc>;

interrupts = <8>;

interrupt-names = "irq_hack";

status = "okay";

};

"The driver code to register irq"

irq = platform_get_irq_byname (pdev, "irq_hack");

        if (irq < 0) {

                dev_err(&pdev->dev, "Couldn't register given IRQ\n");

                return -EINVAL;

        }

printk(KERN_DEBUG "gpio_irq_hack: registering IRQ %d\n", irq);

int ret = request_irq(irq, &gpio_irq_hack_handler, IRQF_TRIGGER_FALLING, "gpio_irq_hack", NULL);

if (ret) {

     printk(KERN_ERR "gpio_irq_hack: cannot register IRQ %d ret:%d\n", irq, ret);

     return -EIO;

}

Any suggestion how can it be fixed.

标签 (2)
0 项奖励
回复
1 回复

1,466 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anees

these new kernels may be supported on community,

suggest to post this on meta-fsl-arm mailing list, so that someone

familiar with them could try to assist you. Latest official FSL release is 2.6.22 from

i.MX27 Product Development Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复