i.MX233 and SDIO multiplex

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX233 and SDIO multiplex

ソリューションへジャンプ
3,159件の閲覧回数
daveshah
Contributor I

Would it be possible to have both an SDIO wireless device and an SDHC card on one SSP of the i.MX233, using a multiplexer like TS3A27518E-Q1 or MAX4996? Also, could you do it simply by connecting the data lines together for the two cards and having separate CMD lines for each device?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,733件の閲覧回数
JackyAtFreescal
Senior Contributor II

Quote from "SD Specifications Part 1 Physical Layer Specification Version 2.00"

3.5 Bus Topology

...

Common bus signals for multiple card slots are not recommended. A single SD bus should

connect a single SD card.

...

Regards,

Jacky

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,733件の閲覧回数
YixingKong
Senior Contributor IV

Hi David, did Jacky's answer helps you. If yes, please mark it as Correct Answer.

0 件の賞賛
返信
2,734件の閲覧回数
JackyAtFreescal
Senior Contributor II

Quote from "SD Specifications Part 1 Physical Layer Specification Version 2.00"

3.5 Bus Topology

...

Common bus signals for multiple card slots are not recommended. A single SD bus should

connect a single SD card.

...

Regards,

Jacky

0 件の賞賛
返信